About VishayBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade ShowsVishay History

< Back  
Vishay Releases Industry-First Gen. 5.0 High-Performance 45-V Schottky Diodes Offering Maximum Junction Temperature to +175 °C

New Devices Built on Sub-Micron Trench Technology Feature Very Low Typical Forward Voltage Drop from < 0.50 V at 60 A to < 0.54 V at 30 A, Extremely Low Reverse Leakage from 2 mA to 5 mA at +125 °C


Gen. 5.0 Schottky

Products mentioned:

30CTT045
60CPT045

This release in:

MALVERN, PENNSYLVANIA — July 11, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today launched two new Gen. 5.0 High-Performance 45-V Schottky diodes that are the industry’s first such devices to offer maximum junction temperature to +175 °C. Built on sub-micron trench technology, the 30CTT045 and 60CPT045 devices offer extremely low forward voltage drop and low reverse leakage, allowing designers to increase power density in automotive and other high-temperature applications.

The two Schottky diodes released today feature very low maximum forward voltage drops at +125°C of < 0.50 V typical at 30 A for the 2 x 30 A 60CPT045, and < 0.50 V typical at 15 A for the 2 x 15 A 30CTT045. Reverse leakage at +125°C is an extremely low 5 mA and 2 mA for these respective devices, with very tight parameter distribution. Both devices offer optimized VF versus IR trade-off for increased system efficiency.

The 30CTT045 and 60CPT045 are optimized for ac-to-dc secondary rectification, flyback, buck and boost converters, half-bridge, reverse battery protection, freewheeling, class-D amplifiers, and dc-to-dc module applications. Typical end products include high power density SMPS; adaptors for desktop PCs; servers; automotive drives and controls; consumer electronics like PDPs, LCDs, and high-efficiency audio systems; and mobile electronics such as notebook computers, cell phones, and portable media players.

For designers, the new devices are offered in small RoHS-compliant packages for improved cost-to-power ratios, with RBSOA available for tight and cost-effective designs. The 30CTT045 is offered in the TO-220 package, while the 60CPT045 is offered in the TO-247.

A high and stable breakdown voltage (> 57 V typical) accommodates voltage spikes and optimizes power density, which is increased in the diodes by 25 %. The devices feature 40 % increased ruggedness for reverse avalanche capability, with parts 100 % screened in avalanche, and negligible switching losses.

Samples and production quantities of the new 30CTT045 and 60CPT045 Schottky diodes are available now, with lead times of six to eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword