VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2008 Releases:Vishay’s Improved S-Series High-Precision Bulk Metal® Foil Resistors
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/resistors-discrete/ultra-high-precision/sales
 

Vishay’s Improved S-Series High-Precision Bulk Metal® Foil Resistors Combine TCR of ±2.0 ppm/°C, Tolerances of ±0.005 % (50 ppm) and Load Life Stability of ±0.005 % (50 ppm)

New Devices Deliver High Reliability, Long Lifetimes, Stable Operation in Harsh Conditions, and Instantaneous Thermal Stabilization Time

MALVERN, Pa. — July 30, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the improved S series of high-precision Bulk Metal® foil (BMF) resistors, which provide a military-grade typical TCR of ±2 ppm/°C from -55 °C to +125 °C, +25 °C ref., tolerance of ±0.005 %, and load life stability of ±0.005 % for more than 10,000 hours.

The S series comprises 12 model numbers with resistance values from 0.5 Ω to 1 MΩ, with any resistance value available at any tolerance within the resistance range at no additional cost or lead time effect. The devices are rated for power levels up to 2 W at 70 °C and can withstand electro-static discharges (ESD) in excess of 25 kV. Rise time for the S series devices is a nearly immeasurable 1 ns without ringing.

Devices in the S series are built to handle unconventional environmental conditional conditions with minimal drift, making them well suited for military/space applications according to EEE-INST-002 specifications and MIL-PRF 55182. The ultimate resistor component for analog applications, the construction of S series resistors guarantees a high level of reliability, stable operation in harsh conditions, and high resistance to thermal shock, mechanical shock, and vibrations. Each S series resistor undergoes a short time overload test of 6.25 times the rated power during the manufacturing process.

The new devices are resistant to moisture as well, and are designed with a coating and molding compound that provides water proofing, moisture proofing, and mechanical damping, as well as a path for heat dissipation.

The S series allows designers to achieve much better performance by combining a range of high-precision specifications in a single device. In addition to its low TCR, tolerance, and load life stability values, the S series offers a low voltage coefficient of < 0.1 PPM/V; current noise of < -42 dB; and thermal EMF of 0.05 µV/ °C. S series resistors offer fast thermal stabilization of less than 1 second, and a non-inductive (< 0.08 µH), non-capacitive design.

Typical applications for the S series devices will include dc-to-dc converters, feedback circuits, and precision amplifiers in test and measurement instrumentation, medical systems, satellites and aerospace systems, commercial and military avionics, weapons systems, audio systems, and high-temperature systems including down-hole drilling.

Both leaded and surface-mount (SMR1D and SMR3D) S series resistors are available now, with lead times of 72 hours for samples, and three weeks for standard orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
S series
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account