|
For more information: New Vishay Siliconix 8-V to 30-V P-Channel PowerPAK SC-75 Power MOSFETs Feature On-Resistance as Low as 0.052 Ohms in 1.6-mm by 1.6-mm Footprint Area
MALVERN, PENNSYLVANIA — August 20, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today released a family of p-channel power MOSFETs in the PowerPAK SC-75, including several devices rated from 8 V to 30 V that are industry-firsts for their voltage ratings in this package type. Among the devices being released today are the industry.s first -12-V (SiB419DK), and -30-V (SiB415DK) single p-channel power MOSFETs in the PowerPAK SC-75 package. The previously announced SiB417DK is the first such -8-V device and is joined today by an ESD-protected version with the same -8-V rating, the SiB417EDK. Both of these 8-V devices include on-resistance specifications down to VGS = 1.2 V, potentially allowing designers to reduce space requirements, power consumption, and solution cost by eliminating the need for level-shift circuitry. The new products also include two -20-V devices, the single SiB411DK and dual SiB911DK. On-resistance for the single devices at a 4.5-V gate drive ranges from 0.052 ohms to 0.066 ohms. The Vishay Siliconix PowerPAK SC-75 power MOSFETs measure 1.6 mm by 1.6 mm by 0.75 mm — the same area dimensions as the standard SC-75 — but offer much lower on-resistance thanks to a construction that accommodates a larger die within the same footprint. In addition to helping the environment by saving energy, the PowerPAK SC-75 is 100 % lead (Pb)-free, halogen-free, and RoHS-compliant, meeting the demands of international legislation for elimination of hazardous substances. The new PowerPAK SC-75 devices offer a new miniaturized package option to designers who are looking for ways to save space and reduce power consumption in portable electronic systems that are continually increasing in functionality. To meet consumer expectations for battery run times between charges, designers require smaller MOSFET packages with low power consumption, and this is just what the new PowerPAK SC-75 devices provide. Typical applications for the p-channel PowerPAK SC-75 power MOSFETs will include load switching in cell phones, PDAs, digital cameras, MP3 players, and smart phones. The -30-V SiB415DK will also be used for load switching and driving white LEDs in notebook computers and other portable devices. Product datasheets: Samples and production quantities of the new PowerPAK SC-75 power MOSFETs are available now, with lead times of 10 to 12 weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. PowerPAK is a registered trademark of Siliconix incorporated. |