|
For more information: Vishay Releases Three New X2 EMI Suppression Film Capacitors With Increased Voltage Rating to 310 VACDevices Offer Wide Lead Pitch Range From 7.5 mm to 27.5 mm and Capacitance Values From 1 nF to 4.7 μF
MALVERN, PENNSYLVANIA — Sept. 26, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of three new X2 electromagnetic interference (EMI) suppression film capacitors with an increased maximum mains voltage of 310 VAC and a wide range of lead pitches and capacitance values. While most standard EMI suppression film capacitors provide a voltage rating of 275 VAC to 305 VAC, Vishay's new MKP 339 X2, MKP 338 2 X2, and MKP 336 2 X2 devices offer designers an increased voltage rating while continuing to meet safety approvals and maintaining the same compact dimensions. Utilizing the latest film technology to offer lead pitches from 7.5 mm to 27.5 mm, capacitance values from 1 nF to 4.7 μF, and a permissible DC voltage of 630 V, the capacitors are optimized for standard across the line applications (50/60 Hz) in power supplies, electronic ballasts, EMI filters, CRT and LCD TVs and monitors, and white goods. Climatic tested according to EN 60068-1 (55/110/56/B), the encapsulation of the devices consists of a flame retardant UL-class 94 V-0 plastic case, which is epoxy resin sealed. Supplied loose in box or taped on ammopack or reel, the lead (Pb)-free capacitors are RoHS-compliant and feature tinned wire leads. Device Specification Table:
Samples and production quantities of the new X2 EMI suppression film capacitors are available now, with lead times of 8 to 10 weeks for larger orders. Pricing varies by capacitance value and lead pitch.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.
|