|
For more information: Vishay’s New USB-OTG Bus Port Protection Array Provides Low Typical Capacitance of 0.7 pF and Low Maximum Leakage Current Down to 0.085 μA in Ultra-Compact LLP75-7L Leadless PackageDevice Features Low Profile of 0.6 mm for Board Space Savings in Portable Electronics
MALVERN, Pa. — Nov. 14, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today released a compact new ESD-protection array featuring a low capacitance and leakage current to protect USB-OTG ports against transient voltage signals. The new device provides three lines of USB ESD protection at a 5.5-V working range, and one line of VBUS protection at a 12-V working range. The VBUS053AZ-HAF is packaged in the leadless LLP75-7L, with a 1.6-mm by 1.6-mm footprint and an ultra-low profile of 0.6 mm to minimize the board space required for active ESD protection in high-speed data applications, such as USB 2.0 and HDMI in HDTVs and mobile electronics, including portable gaming systems, MP3 players, and cell phones. The new device features a low load capacitance of 0.7 pF for the three data lines D+, D-, and ID, and a low maximum leakage current of 0.085 μA at the working voltage of 3.3 V, and 1 μA at 5.5 V. The VBUS053AZ-HAF offers a low maximum clamping voltage of less than 4.1 V at 3 A for the data lines, and less than 30 V at 8 A for the VBUS line. The bus port protection array provides transient protection as per IEC 61000 4 2 (ESD) at 15 kV (air and contact discharge), and IEC 61000 4 5 (lightning) from 3 A. The lead (Pb)-free device features a halogen-free molding compound, and is compliant with RoHS 2002/95/EC and WEEE 2002/96/EC. Samples of the new USB-OTG bus port protection array in the compact LLP75-7L package are available now. Production quantities will be available in Q4 2008, with lead times of ten weeks for large orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.
|