Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay’s New 2-Line and 4-Line Bus Port Protection Arrays Provide Low Typical Capacitance of 0.8 pF and Low Leakage Current of < 0.1 μA in Ultra-Compact LLP2513 and LLP1713 Leadless Packages

Devices Feature “Flow Through” Design and Low Profile of 0.6 mm for High-Speed Data Lines in Portable Electronics


VBUS

Products mentioned:

VBUS052CD-FAH
VBUS054CD-FHI
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

Malvern, Pennsylvania — Dec. 12, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today released two new compact 2-line and 4-line ESD-protection arrays with low capacitance and leakage current for the protection of high-speed data lines against transient voltage signals.

Featuring an ultra-low profile of 0.6 mm for board space savings, the two-line VBUS052CD-FAH is packaged in the leadless LLP1713, while the 4-line VBUS054CD-FHI is packaged in the LLP2513. The protection arrays feature a “flow through” design that supports the surge resistance requirements for high-speed data lines in applications such as USB 2.0, HDMI, display ports, eSATA, and 1394/Firewire in HDTVs and mobile electronics, including portable gaming systems, MP3 players, and cell phones.

The new devices feature a low load capacitance of 0.8 pF and a low maximum leakage current of < 0.1 μA at the working voltage of 5 V. The arrays offer a breakthrough voltage of typical 7.9 V (at 1 mA), and a maximum clamping voltage of 15 V at 3.5 A.

The bus port protection arrays provide transient protection for data lines as per IEC 61000 4 2 (ESD) at 15 kV (air and contact discharge). The lead (Pb)-free devices offer pure tin pin plating and a halogen-free molding compound, and their soldering can be checked by standard vision inspection without X-rays. The arrays are compliant with RoHS 2002/95/EC and WEEE 2002/96/EC.

Samples of the new 2-line and 4-line ESD bus port-protection arrays are available now. Production quantities will be available in Q1 2009, with lead times of 10 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword