Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay Siliconix Releases New 20-V N-Channel Power MOSFET Plus Schottky Diode With Industry’s Smallest Footprint of 1.6 mm by 1.6 mm

SiB800EDK Combines Schottky with Low Forward Voltage of 0.32 V and MOSFET with Low 0.960-Ω On-Resistance at 1.5-V VGS in PowerPAK® SC-75 Package


SiB800EDK

Products mentioned:

SiB800EDK
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — Dec. 12, 2008 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the industry’s smallest 20-V n-channel power MOSFET plus Schottky diode. Featuring the 1.6-mm by 1.6-mm thermally enhanced PowerPAK® SC-75 package, the SiB800EDK combines a Schottky diode with a low forward voltage of 0.32 V at 100 mA and a MOSFET with on-resistance ratings specified at gate drives down to 1.5 V.

As portable electronics become more compact, the size of components becomes critical. With its ultra-compact footprint, the SiB800EDK is 36 % smaller than devices in 2-mm by 2-mm packages, while offering an ultra-thin 0.75-mm profile. The integration of two components into one package not only saves space, but the inclusion of a trench Schottky keeps the forward voltage low, reducing voltage drop in level shift applications.

The SiB800EDK offers low on-resistance values from 0.960 Ω at 1.5-V VGS to 0.225 Ω at 4.5-V VGS. The low on-resistance rating at 1.5 V allows the MOSFET to be used with signals at low levels.

Typical applications for the new device will include level shift switching in I2C interface and boost converters in portable devices such as cell phones, PDAs, digital cameras, MP3 players, and smart phones.

The SiB800EDK features ESD protection, and is 100 % lead (Pb)-free, halogen-free, and RoHS-compliant, meeting the demands of international legislation for elimination of hazardous substances.

Samples and production quantities of the new SiB800EDK are available now, with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

PowerPAK is a registered trademark of Siliconix incorporated

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword