|
For more information: Vishay Siliconix Releases Industry’s First 190-V N-Channel Power MOSFET Plus 190-V Co-Packaged Power Diode With Compact 2-mm by 2-mm Footprint and Low 0.75-mm ProfileSiA850DJ is Industry’s First Device to Feature On-Resistance Rating at 1.8-V VGS for High-Voltage Applications
MALVERN, PENNSYLVANIA — Jan. 7, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the industry’s first 190-V n-channel power MOSFET plus co-packaged 190-V power diode with a compact 2-mm by 2-mm footprint and an ultra-thin 0.75-mm profile. Offered in the PowerPAK® SC-70 package, the SiA850DJ is also the industry’s first such device with an on-resistance rating at 1.8-V VGS. Typical applications for the SiA850DJ will include boost dc-to-dc converters for high-voltage piezo-electric motors and organic LED (OLED) backlighting in portable devices such as cell phones, PDAs, MP3 players, and smart phones. Integrating the MOSFET and the power diode into the same package saves designers at least one third of the PCB area, while at the same time lowering solution costs by eliminating the need for an external diode. While larger devices feature on-resistance ratings down to 2.5 V, the SiA850DJ is rated down to 1.8 V, which further saves board space by reducing the need for level shift circuitry. The device offers low on-resistance values from 17 Ω at 1.8-V VGS to 3.8 V at 4.5-V VGS, and a diode forward voltage of 1.2 V at 0.5 A. The SiA850DJ is 100 % lead (Pb)-free, halogen-free, and RoHS-compliant, meeting the demands of international legislation for elimination of hazardous substances. Samples and production quantities of the new SiA850DJ are available now, with lead times of 10 to 12 weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. PowerPAK is a registered trademark of Siliconix incorporated |