Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay Releases Compact SMD IR Receiver With 0.5-mW/sqm Typical Irradiance and 300-μs Reaction Time for Sensor and Light Barrier Systems

Fixed Gain Device is Insensitive to Supply Voltage Ripple and EMI Noise, and Offers Low Supply Current of 0.85 mA


TSOP5038

Products mentioned:

TSOP5038
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

Malvern, Pennsylvania — Jan. 16, 2009 — Vishay Intertechnology (NYSE: VSH) broadens its optoelectronics portfolio with the introduction of a compact SMD IR receiver optimized for sensor and light barrier systems. With its fast reaction times, insensitivity to supply voltage ripple and EMI noise, and low supply current of 0.85 mA typical at 5 V, the fixed gain device provides consistent performance in all ambient light conditions.

In mid- to long-range reflective sensor systems and IR light barrier systems, such as garage door openers, urinals, and other “presence of object” systems, gain control must be handled differently than in remote applications. In remote applications, the automatic gain control (AGC) adjusts the gain in response to ambient light levels, spurious noise, and other criteria in order for the receiver to continue responding to the data signal while rejecting stray noise. But variable gain is not desired in sensor applications, as this greatly complicates the design. In addition, sensor applications require fast reaction times in order to operate at a continuous 38-kHz signal.

The TSOP5038 solves both of these problems by offering a high fixed gain in all ambient light environments, and allows a short burst repetition time that results in a fast 300-μs reaction time. Continuous signals at 38 kHz or 38 kHz bursts may be used to drive the IR emitter. To simplify the design, an internal IR filter suppresses visible light.

To further simplify designs, the TSOP5038 features a photo detector and preamplifier in one package. The highly sensitive device offers a 0.5-mW/sqm typical irradiance and a supply voltage from 2.7 V to 5.5 V. The receiver is complaint with RoHS 2002/95/EC and WEEE 2002/96/EC.

Samples and production quantities of the TSOP5038 are available now, with lead times of eight weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword