Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay Releases Industry’s First TrenchFET® Power MOSFET in MICRO FOOT® Chipscale Package to Feature Backside Insulation


Si8422DB

Products mentioned:

Si8422DB
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — Jan. 21, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today released the industry’s first TrenchFET® power MOSFET in the chipscale MICRO FOOT® package to feature backside insulation.

The Si8422DB is optimized for power amplifier, battery, and load switching in portable devices such as cell phones, PDAs, digital cameras, MP3 players, and smart phones. The 2-mil backside coating of the device insulates the top of the MICRO FOOT package to electrical shorts from being created by temporary contact with moving parts in portable devices.

This insulation allows the device to be used in applications with very thin height requirements, providing designers with the flexibility to place the MOSFET where other items may be directly above it, such as shielding, buttons, or touch screens, which further compress the product height when depressed. This layout flexibility also translates into reduced parasitics, as the traces can be better optimized by not having to be routed to areas on the PCB with less height restrictions.

The 20-V n-channel Si8422DB features an ultra-compact 1.55-mm by 1.55-mm footprint with a slim 0.64-mm profile. The device offers a low on-resistance range from 0.043 Ω at 1.8-V VGS to 0.037 at 4.5-V VGS, with a maximum gate-source voltage of ±8 V.

Samples and production quantities of the new Si8422DB are available now, with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

TrenchFET and MICRO FOOT are registered trademarks of Siliconix incorporated

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword