|
For more information: Vishay Releases Industry’s First Winged Low-Profile, High-Current Inductor in 4040 Case Size With High Maximum Frequency to 1.0 MHz and Low DCR Down to 0.64 Milliohms TypicalFor Cut-Out PCBs, New IHLW-4040CF-11 Inductor Offers Low Profile of 1.2 mm for Both Sides of the Board
MALVERN, PENNSYLVANIA — April 15, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the industry’s first winged low-profile, high-current inductor in the 4040 case size. Designed to be placed on a cut-out PCB, the IHLW-4040CF-11 offers designers a high-current solution using a larger part, without exceeding a profile of 1.2 mm on either side of the PC board. With a frequency range up to 1.0 MHz, the new IHLP® inductor serves as a high-performing, space- and power-saving solution for voltage regulator module (VRM) and dc-to-dc converter applications in end products including next-generation mobile devices; notebooks, desktop computers, servers, graphic cards, portable gaming devices, personal navigation systems, personal multimedia devices, and automotive systems; low-profile, high-current power supplies and point of load (POL) converters; distributed power systems; and field-programmable gate arrays (FPGAs). The IHLW-4040CF-11 offers an inductance range from 0.10 μH to 2.2 microhenries, a saturation current range from 14.0 A up to 48 A, heat rating current from 16 A to 46 A, typical DCR from 0.64 milliohms to 6.83 milliohms, and maximum DCR from 0.70 milliohms to 7.21 milliohms. The new inductor handles high transient current spikes without hard saturation. Packaged in an RoHS-compliant, 100 % lead (Pb)-free shielded, composite construction that reduces buzz noise to ultra-low levels, the new device is specified for an operating temperature range of 55 deg. C to +125 deg. C, with high resistance to thermal shock, moisture, mechanical shock, and vibration. Samples and production quantities of the new inductor are available now, with lead times of 10 to 12 weeks for large orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. IHLP is a registered trademark of Vishay Dale Electronics, Inc. |