Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay Releases Two New Schottky Rectifiers With Ultra-Low 0.35-V Forward Voltage Drops in the Miniature MicroSMP Power Package

Devices Feature High-Current-Density Performance up to 30 V and 1 A in Space-Saving 2.7-mm by 1.4-mm Footprint


MicroSMP

Products mentioned:

MicroSMP
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA. — April 15, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today launched two new Schottky rectifiers with ultra-low forward voltage drops of 0.35 V at + 85 °C and 0.4 V at + 25 °C. Featuring the miniature MicroSMP power package and voltage ratings of 20 V (MSS1P2U) and 30 V (MSS1P3U) at 1 A, the devices provide high current power density and low thermal resistance to enable space-saving designs.

The MicroSMP package of the MSS1P2U and MSS1P3U measures only 2.7 mm by 1.4 mm, with a 0.68-mm profile. Combined with the devices’ high current density of 1 A, the rectifiers are designed to provide more power in a smaller space for snubbers in hard disk drives for notebook computers, LCD TVs, and desktop TVs; secondary rectifiers for miniature switchmode power supplies and adaptors, and power supply type battery chargers; polarity protection for hand-held equipment, such as PMPs, digital cameras, MP3 players, navigation systems, GPS, and cell phones; and polarity protection of power lines and signal lines in automotive and industrial systems.

The MSS1P2U and MSS1P3U feature a peak forward surge current of 30 A and maximum junction temperature of + 125 °C. Ideal for automated placement, the rectifiers meet MSL level 1, per J-STD-020, LF maximum peak of + 260 °C. The devices are RoHS complaint in accordance with 2002/95/EC and WEEE 2002/96/EC, and are halogen-free according to IEC 61249-2-21.

Samples and production quantities of the MSS1P2U and MSS1P3U rectifiers are available now, with lead times of eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword