Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay Releases Industry’s First Wet Tantalum Capacitors in True Surface-Mountable, Molded Package

M34 and M35 Devices Offer Wide Capacitance Range of 1.7 μF at 125 V to 220 μF at 6 V, ± 20 % Standard Capacitance Tolerance, and Operate Up To + 125 °C With Voltage Derating


M34 and M35

Products mentioned:

M34
M35
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — April 22, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of two new wet tantalum capacitors that are the industry’s first such devices to be offered in a true surface-mountable molded package.

The M34 and M35 wet tantalum electrolytic chip capacitors incorporate the advantages of all the varieties of electrolytic capacitors and eliminate most of the disadvantages. The devices have a higher ripple current capability than any other electrolytic type with similar combinations of capacitance and case size. In addition, the M35 features a 3-V reverse voltage capability at + 85 °C.

Optimized for power supplies in all avionics, military, and space applications that currently use Vishay’s ST -T1 (M34) or 135D- C/T1 (M35) case ratings, the devices’ new surface-mountable case allows designers to eliminate the last through-hole component on their PCB, reducing overall PCB assembly cost.

With a wide capacitance range of 10 μF at 125 V to 120 μF at 25 V for the M34, and 1.7 μF at 125 V to 220 μF at 6 V for the M35, the devices feature all industry-standard T1 wet tantalum ratings. The capacitors offer tin/lead or 100 % tin (RoHS- complaint) terminations.

The M34 and M35 operate over a temperature range of - 55 °C to + 85 °C, and up to + 125 °C with voltage derating. The devices offer a ± 20 % standard capacitance tolerance at 120 Hz and + 25 °C, with tolerances of ± 5 % and ± 10 % also available.

Samples and production quantities of the new surface mountable, wet tantalum capacitors are available now, with lead times of approximately 20 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword