Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay Siliconix Extends P-Channel TrenchFET® Gen III Technology to Ultra-Small Packages, Lowering On-Resistance Up to 44 % With New Dual 20-V Power MOSFET in 2-mm by 2-mm Footprint Area


SiA921EDJ

Products mentioned:

SiA921EDJ
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — April 30, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new dual 20-V p-channel TrenchFET® Gen III power MOSFET with the lowest on-resistance ever achieved for a dual p-channel device in the thermally enhanced PowerPAK® SC-70 2-mm by 2-mm footprint area.

With the SiA921EDJ, Vishay extends its p-channel TrenchFET Gen III technology to ultra-small packages for handheld electronics. The new device will be used for dc-to-dc buck converters, as well as load, PA, and battery switches in portable devices such as cell phones, smart phones, PDAs, and MP3 players. The lower on-resistance of the SiA921EDJ translates into lower power consumption, saving power and prolonging battery life between charges in these devices.

The SiA921EDJ offers an ultra-low on-resistance of 59 mΩ at 4.5 V and 98 mΩ at 2.5 V. The low on-resistance of the TrenchFET Gen III MOSFET translates into lower conduction losses, allowing the device to perform switching tasks with less power than any previous dual p-channel power MOSFETs on the market.

The closest competing p-channel device with a ≥ 12-V gate-to-source rating features on-resistance of 95 mΩ at a 4.5-V gate drive and 141 mΩ at 2.5 V. These values are 38 % and 44 % higher, respectively, than the SiA921EDJ. The compact 2-mm by 2-mm footprint of the PowerPAK SC-70 is half the size of the TSOP-6, while offering comparable on-resistance.

The MOSFET is halogen-free in accordance with IEC 61249-2-21.

Samples and production quantities of the new SiA921EDJ TrenchFET power MOSFET are available now, with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

TrenchFET and PowerPAK are registered trademarks of Siliconix incorporated

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword