|
For more information: Latest Vishay Siliconix Billion-Cell Per Square Inch P-Channel TrenchFET® Gen III Power MOSFET Offers Industry-Low On-Resistance in PowerPAK® SC-75Latest Device in Breakthrough TrenchFET Gen III Family Extends Package Options from PowerPAK SO-8 Down to Ultra-Small 1.6-mm by 1.6-mm Footprint Area
MALVERN, Pa. — Sept. 10, 2009 — Vishay Intertechnology, Inc. (NYSE) today introduced a new 20-V p-channel power MOSFET with the lowest on-resistance ever achieved for a p-channel device a 1.6-mm by 1.6-mm footprint area. The new SiB457EDK is built on TrenchFET® Gen III p-channel technology, which uses self-aligning process techniques to pack one billion transistor cells into each square inch of silicon. This leading edge technology allows a super fine, sub-micron pitch process that cuts the industry’s best on-resistance for a p-channel MOSFET nearly in half. With the release of this new device, TrenchFET Gen III p-channel power MOSFETs are now available in four surface-mount package types, including the thermally enhanced PowerPAK® SO-8, which offers industry’s lowest on-resistance down to 1.9 mΩ in an SO-8 footprint area. The smallest device in the family so far, the SiB457EDK in the PowerPAK SC-75 features the industry’s lowest on-resistance in a 1.6-mm by 1.6-mm footprint area. Its rDS(on) values range from 35 mΩ at 4.5 V to 130 mΩ at 1.5 V. These new SiB457EDK values are up to 42 % lower at 4.5 V and 2.5 V, and 46 % lower at 1.8 V than the closest competing p-channel device with the same voltage ratings. TrenchFET Gen III p-channel MOSFETs help to save energy in applications such as adaptor and load switches in notebook computers and industrial/general systems as well as load switches in charging circuits and portable devices such as cell phones, smart phones, PDAs, and MP3 players. The low on-resistance provided by the milestone billion cells per square inch technology translates into lower conduction losses, saving power and prolonging battery life between charges. The following table summarizes the key specifications for the TrenchFET Gen III p-channel devices released to date.
Vishay Siliconix was the industry’s first supplier to introduce Trench power MOSFETs. The company’s TrenchFET intellectual property includes numerous patents, including fundamental technology patents dating from the early 1980s. Each new generation of TrenchFET technology yields products that raise the bar for power MOSFET performance in a wide range of computing, communications, consumer electronics, and many other applications. The SiB457EDK specifies on-resistance ratings at four gate-to-source voltages, including a 1.5-V rating that enables designs with smaller input voltages to implemented with a higher safety margin. Its compact PowerPAK SC-75 package, meanwhile, reduces the space required for power circuitry, opening up real estate for other product features or enabling a smaller end product. The SiB457EDK also includes ESD protection of 2500 V typical to enable field failures reductions, while exhibiting low leakage current of only 5 μA at VGS = 8 V. The p-channel TrenchFET Gen III power MOSFET family is halogen-free in accordance with IEC 61249-2-21, compliant to RoHS Directive 2002/95/EC, and 100 % Rg- tested. Further information on the family is available at http://www.vishay.com/mosfets/geniii-p/. Samples and production quantities of the new SiB457EDK TrenchFET power MOSFET are available now, with lead times of 10 to 12 weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. TrenchFET and PowerPAK are registered trademarks of Siliconix incorporated |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||