Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay’s New User-Configurable Planar Transformer Features Frequency Range of 50 kHz to 400 kHz, Handles up to 220 W for SMPS Applications


PLAC 100 transformers

Products mentioned:

PLAC 100
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — Sept. 14, 2009 — Vishay Intertechnology Inc. (NYSE: VSH) today announced a versatile new planar transformer designed for switchmode power supply (SMPS) applications, including flyback, forward, push-pull, and half-bridge converters.

Delivering a high level of flexibility, the new Vishay Sfernice PLAC 100 is user-configurable with software supplied by Vishay, which allows designers to adapt the transformer to a wide range of applications by setting the power supply type and desired level of input voltage, output voltage, power, and frequency. Once these variables are entered, the software does the rest of the work, automatically determining the appropriate configuration and determining which outputs should be connected to obtain the best performance.

Typical applications for the PLAC 100 will include military, avionic, and medical systems, where its user configurability will save on engineering resources, speed time to market, and reduce sourcing and inventory costs by allowing a single component to cover a wide range of applications and power values.

The frequency range for the PLAC 100 is 50 kHz to 400 kHz. The transformer can handle up to 220 W. SMD and through-hole versions are available, with an operating temperature range of − 55 °C to + 125 °C.

Samples and production quantities of the PLAC 100 are available now with lead times of six to eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword