Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay’s New 1-mm by 1-mm Maximum MICRO FOOT® Devices Are Industry’s Smallest Chipscale MOSFETs; Include First Device Under 1.2 mm2 with 12-V Gate-to-Source Voltage


Si8461DB Si8465DB pmos

Products mentioned:

Si8461DB
Si8465DB
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — Oct. 16, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today released two MICRO FOOT® power MOSFETs with maximum dimensions of 1 mm by 1 mm by 0.548 mm, which sets a new milestone as the smallest chipscale power MOSFETs yet.

The 20-V p-channel Si8461DB and Si8465DB will be used for load switch, battery switch, and charger switch applications in a wide range of portable devices, where their small size and height will help reduce the space occupied by power management circuitry and/or enable more functionality. Compared to the next smallest chipscale power MOSFET on the market, the 1-mm by 1-mm by 0.548-mm MICRO FOOT has a 9 % smaller footprint.

On-resistance for the Si8461DB is 0.1 Ω at a 4.5-V gate drive, which represents a tenfold improvement over non-chipscale devices with similar footprint dimensions and thus provides a significant opportunity to conserve battery energy in portable devices. In addition to the 4.5-V rating, the Si8461DB is specified for maximum on-resistance values at 2.5 V, 1.8 V, and 1.5 V, which aligns the device with the smaller input signals common in portable systems. For applications requiring higher input voltages such as charger switches, the Si8465DB has a gate-to-source voltage of 12 V; on-resistance is 0.104 Ω at a 4.5-V gate drive and 0.148 Ω at 2.5 V.

Samples and production quantities of the Si8461DB and Si8465DB are available now, with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

MICRO FOOT is a registered trademark of Siliconix incorporated

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword