|
For more information: New Vishay Sfernice P11L Panel Potentiometer Features Long Life of 2 Million Cycles and Compact
|
| For more information: Media contact - Andrew Post, Sr. Manager, Global Communications Phone: 1.610.251.5287 Fax: 1.610.889.9429 E-mail: andrew.post@vishay.com Sales contact: |
MALVERN, Pa. — Nov. 4, 2009 — Vishay Intertechnology Inc. (NYSE: VSH) today announced a new economical, long-life panel potentiometer
featuring up to four modules and a compact
While standard low-cost panel potentiometers reach 50,000 cycles, the P11L offers a long life of 2 million cycles. For designers, this reduces the need for replacement parts, increasing reliability and lowering maintenance costs.
The versatile panel potentiometer is optimized for CMOS amplifier gain, CMOS IC offset setting, motor speed control, and angle sensor applications in welding machines, air conditioning units, tooling machines, medical systems, X-ray equipment, trucks and tractors, and military and avionics systems.
With its
The P11L features up to four modules, a choice of
The Vishay Sfernice potentiometer offers a typical operating torque from
Compliant to RoHS directive
Samples and production quantities of the new P11L are available now, with lead times of four to eight weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.