|
For more information: Vishay Extends Resistance Range of E/H MIL-55342-Qualified Resistor Chips in Compact 2208, 2010, and 2512 Case Sizes to
|
|||||||||||||||||||||||||||
| For more information: Media contact - Andrew Post, Sr. Manager, Global Communications Phone: 1.610.251.5287 Fax: 1.610.889.9429 E-mail: andrew.post@vishay.com Sales contact: |
MALVERN, Pa. — Nov. 13, 2009 —Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it has extended the resistance
range of its E/H MIL-PRF-55342-qualified thin film resistor chips in the compact 2208, 2010, and 2512 case sizes. Allowing for lower resistance
values in high-reliability applications, the enhanced devices feature ratings down to
Intended for high-reliability military and aerospace applications with stringent performance requirements, the enhanced E/H resistor chips offer stable film and performance characteristics of
The resistors’ all-sputtered wraparound terminations ensure excellent adhesion and dimensional uniformity. Exact dimensions
and clean, straight edges are produced by a precise wafer-sawing process. The E/H devices’ electroplated nickel barrier layer enables operation at temperatures up to
In addition to very low noise of less than
Device Specifications Table
| Part | Case Size |
|
|
|
|
|---|---|---|---|---|---|
|
|
|
||||
| M55342/05 | 2208 | 175 | 225 |
|
|
| M55342/08 | 2010 | 150 | 800 |
|
|
| M55342/09 | 2512 | 200 | 1000 |
|
|
The E/H devices provide a shelf-life stability of
Samples and production quantities of the new devices are available now, with lead times of eight weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.