|
For more information: Vishay Siliconix
|
| For more information: Media contact - Bob Decker, Wall Street Communications Phone: 1.415.409.0233 Fax: 1.650.618.1512 E-mail: bob.decker@wallstcom.com Sales contact: |
MALVERN, PENNSYLVANIA — Nov. 18, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new
The SiA433EDJ offers an ultra-low on-resistance of
The new MOSFET is also the only
The SiA433EDJ will be used as load, battery, and charging switches in handheld devices such as cell phones, smart phones, PDAs, and MP3
players. The low on-resistance of the MOSFET translates into lower conduction losses, saving power and prolonging battery
life between charges in these devices. At half the size of the
To reduce field failures due to ESD, the device features a built-in Zener diode for ESD protection up to
Samples of the new SiA433EDJ TrenchFET power MOSFET are available now. Production quantities will be available in Q1 2010, with lead times of 14 to 16 weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.