|
For more information: Vishay Siliconix
|
| For more information: Media contact - Bob Decker, Wall Street Communications Phone: 1.415.409.0233 Fax: 1.650.618.1512 E-mail: bob.decker@wallstcom.com Sales contact: |
MALVERN, PENNSYLVANIA — Dec. 21, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new
The new SiB455EDK is the latest product built on TrenchFET Gen III
The SiB455EDK offers an
The MOSFET will be used as load, PA, and battery switches in handheld devices such as cell phones, smart phones, PDAs, and
MP3 players. The low on-resistance of the SiB455EDK translates into lower conduction losses, saving power and prolonging battery life between charges in these devices, while
its compact PowerPAK
The new device is also the only
To reduce field failures due to ESD, the device features typical ESD protection of
Samples of the new SiB455EDK TrenchFET power MOSFET are available now. Production quantities will be available in Q1 2010, with lead times of 14 to 16 weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.