Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

New Vishay Siliconix 60-V SiM400 in 1-mm x 0.6-mm SOT-923 Delivers Space Savings for Small-Signal Applications


SiM400 mosfets

Products mentioned:

SiM400
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — Dec. 28, 2009 — Vishay Intertechnology, Inc. (NYSE: VSH) today released a 60-V n-channel power MOSFET in the tiny SOT-923 package that will provide dramatic space savings over devices in larger packages such as the SC-70 and SC-89.

The smallest 60-V power MOSFET ever released, the SiM400’s SOT-923 measures 1 mm by 0.6 mm with a maximum height profile of 0.43 mm. Its footprint dimensions are 77 % smaller than the SC-89, while its height profile is 26 % thinner.

On-resistance for the new device is 3.9 Ω at VGS = 10 V, 4.8 Ω at 4.5 V, and 8 Ω at 3.5 V.

The SiM400 will serve in a very wide range of small-signal switching applications where minimal board space is available, including miniaturized motors in digital still and video cameras, electro-luminescent backlighting, and boost dc-to-dc converters, where its miniscule dimensions will help to save space and/or enable greater functionality.

Handheld devices tend to use small-signal switching in conjunction with complex controllers such as power management units (PMUs). The SiM400’s low on-resistance ratings down to 3.5 V, which is an exceptionally low gate-to-source value for a 60-V device, and its small package size compared to a SC-89, thus represent important benefits.

The environmentally friendly new device is lead (Pb)-free, halogen-free, and RoHS-compliant. It additionally provides ESD protection up to 1500 V.

Samples and production quantities of the SiM400 are available now, with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword