Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay’s New Bidirectional Symmetrical Single-Line ESD Protection Diode Offers Extremely Low Capacitance of 0.3 pF in Ultra-Compact LLP1006 Package

Device Features Low Profile of < 0.4 mm for Board Space Savings in Portable Electronics


VBUS05L1-DD1-G-08 diodes

Products mentioned:

VBUS05L1-DD1-G-08
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — Jan. 8, 2010 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new bidirectional symmetrical (BiSy) single-line ESD protection diode in the LLP1006 package. The compact VBUS05L1-DD1-G-08 provides a very low capacitance of 0.3 pF for the protection of antennas, USB 3.0, and HDMI ports from transient voltage signals in portable electronics.

Featuring a compact 0.6-mm by 1.0-mm footprint with a very low package height of < 0.4 mm, the VBUS05L1-DD1-G-08 minimizes the board space required for active ESD protection in devices such as portable gaming systems, digital cameras, MP3 players, and mobile phones.

At the working voltage of 5.5 V, the diode offers a high isolation to ground characterized by a low leakage current of < 0.1 µA. Any transient voltage signal exceeding the reverse breakthrough voltage of typical 8.4 V at 1 mA will be "clamped" or "short" to ground. The devices features a maximum clamping voltage of 14 V at 1 A.

Due to the short leads and small package size of the LLP1006, the diode’s line inductance is very low, allowing fast transients such as an ESD strike to be clamped with minimal over- or undershoots.

The VBUS05L1-DD1-G-08 provides transient protection for one data line as per IEC 61000-4-2 at ± 9 kV (air and contact discharge). The device is lead (Pb)-free and complies with RoHS 2002/95/EC and WEEE 2002/96/EC. To lower manufacturing costs, soldering of the diode can be checked by standard vision, eliminating the need for X-ray inspection.

Samples and production quantities of the new VBUS05L1-DD1-G-08 are available now, with lead times of eight to ten weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword