|
For more information: Vishay Releases Four New
|
||||||||||||||||||||||||||||||||||||||||||||
| For more information: Media contact - Bob Decker, Wall Street Communications Phone: 1.415.409.0233 Fax: 1.650.618.1512 E-mail: bob.decker@wallstcom.com Sales contact: |
MALVERN, Pa. — Jan. 13, 2010 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced four new
The devices released today include the VSSA310S and VSSA210 in the
With extremely low forward voltage drops down to 0.56 V typical and superior avalanche capability, the devices reduce power
loss and improve efficiency in freewheeling diodes,
The new rectifiers feature a maximum junction temperature of
Device Specification Table:
| Vishay Device | IF (A) | VRRM (V) | VF at IF and TJ | IFSM (A) | TJ max (°C ) | ||
|---|---|---|---|---|---|---|---|
| VF (V) | IF (A) | TA (°C) | |||||
| VSSA210 | 2 | 100 | 0.56 | 2 | 125 | 60 | 150 |
| VSSA310S | 3 | 100 | 0.62 | 3 | 125 | 60 | 150 |
| VSSB310 | 3 | 100 | 0.56 | 3 | 125 | 80 | 150 |
| VSSB410S | 4 | 100 | 0.61 | 4 | 125 | 80 | 150 |
Samples and production quantities of the new Trench MOS Barrier Schottky rectifiers are available now, with lead times of six weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.
TMBS is a registered trademark of Vishay Intertechnology.