|
For more information: Vishay’s New PAT Series of
|
| For more information: Media contact - Andrew Post, Sr. Manager, Global Communications Phone: 1.610.251.5287 Fax: 1.610.889.9429 E-mail: andrew.post@vishay.com Sales contact: |
MALVERN, Pa. — Jan. 15, 2010 —Vishay Intertechnology, Inc. (NYSE: VSH) today introduced the new PAT series of
Featuring a tantalum nitride resistor film on a high-purity alumina substrate, the PAT resistors offer stable film and performance characteristics of 1000 ppm at
Offered with wraparound terminations in eight case sizes from 0402 to 2512, the PAT series offers a resistance range from
The PAT devices are resistant to moisture at
Device Specification Table:
| Case Size | Power Rating (mW) | Working Voltage (V) | Resistance Range (Ω) |
|---|---|---|---|
| 0402 | 50 | 75 | 20 to 35 K |
| 0603 | 150 | 75 | 10 to 80 K |
| 0805 | 200 | 100 | 10 to 301 K |
| 1206 | 400 | 200 | 10 to 1 M |
| 1505 | 400 | 150 | 10 to 1 M |
| 2208 | 750 | 150 | 10 to 1.75 M |
| 2010 | 800 | 200 | 10 to 2 M |
| 2512 | 1000 | 200 | 10 to 3 M |
Samples and production quantities of the PAT resistors are available now, with lead times of eight weeks for standard orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.