|
For more information: Vishay Enhances
|
||||||||||||||||||||||||||||||||||
| For more information: Media contact - Andrew Post, Sr. Manager, Global Communications Phone: 1.610.251.5287 Fax: 1.610.889.9429 E-mail: andrew.post@vishay.com Sales contact: |
MALVERN, PENNSYLVANIA — Jan. 20, 2010 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it has enhanced its
Featuring a cylindrical aluminum case insulated with a blue sleeve and pressure relief in their disc, the
The
As polarized aluminum electrolytic capacitors with a non-solid electrolyte, the
Device Specification Table
| Part # | 101 | 102 |
|---|---|---|
| Case size (D x L in mm) | 35 x 60 to 90 x 220 | |
| Capacitance range | 220 µF to 1 F | |
| Tolerance | ± 20 % | |
| Ripple current | 5.2 A to 49.1 A | 2.1 A to 43.2 A |
| Rated voltage range | 25 V to 100 V | 200 V to 450 V |
| Temperature range | - 40 °C to + 85 °C | |
| Useful life at + 85 °C | 10,000 h (D = 50 mm) 15,000 h (D = 65 mm) |
10,000 h |
| Shelf life at 0 V, + 85 °C | 500 h | |
| Sectional specification | IEC 60384-4/EN130300 | |
| Climatic category IEC 60068 | 40/085/56 | |
Samples and production quantities of the
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.