Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay’s New USB-OTG Bus Port Protection Array Provides Low Typical Capacitance of 0.7 pF and Low Maximum Leakage Current Down to 0.085 µA in Compact LLP1713-9M Leadless Package

Device Provides VBUS Protection at 12-V Working Range


VBUS053BZ-HNH-G-08 usbotg

Products mentioned:

VBUS053BZ-HNH-G-08
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — Mar. 22, 2010 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new ESD-protection array featuring low capacitance and leakage current to protect USB-OTG ports against transient voltage signals. The new VBUS053BZ-HNH-G-08 provides three lines of USB ESD protection at a 5.5-V working range, and one line of VBUS protection at a 12-V working range.

The VBUS053BZ-HNH-G-08 is packaged in the leadless LLP1713-9M, with an ultra-low profile of 0.6 mm to minimize the board space required for active ESD protection in high-speed data applications, such as USB 2.0 and HDMI in HDTVs and mobile electronics, including portable gaming systems, MP3 players, and cell phones.

The new device features a low load capacitance of 0.7 pF for the three data lines D+, D-, and ID, and a low maximum leakage current of 0.085 µA at the working voltage of 3.3 V, and 1 µA at 5.5 V. The array provides a low maximum clamping voltage of > 4.1 V for negative transients and < 18 V for positive transients at 3 A for the data lines. For the VBUS line, the VBUS053BZ-HNH-G-08 features a maximum clamping voltage of 30 V at 8 A.

The VBUS053BZ-HNH-G-08 provides transient protection as per IEC 61000-4-2 (ESD) at 12 kV (air discharge) and 15 kV (contact discharge), with surge current protection in accordance with IEC 6100-4-5 from 3 A.

The lead (Pb)-free device features a halogen-free molding compound, and is compliant with RoHS 2002/95/EC and WEEE 2002/96/EC.

Samples of the new USB-OTG bus port protection array are available now. Production quantities will be available in Q1 2010, with lead times of eight to ten weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword