|
For more information: Vishay Extends MC AT Thin Film Resistor Series with New Case Sizes and Precision VersionsCECC-Approved and AEC-Q200-Compliant Devices Feature 0402 to 1206 Case Sizes, Maximum Permissible Film Temperature of + 175 °C, and Power Ratings Up to 400 mW; Precision Series Offers TCR Down to ± 15 ppm/K and Tolerances to ± 0.1 %
MALVERN, Pa. — Apr. 12, 2010 —Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it has extended its MC AT series of Professional thin film chip resistors to include devices in the 0402, 0603, 0805, and 1206 case sizes. In addition, a new Precision version of the series with lower TCR and tolerances has been released. An increasing number of electronic designs require components that can withstand the effects of high temperature and humidity, which can affect device stability and performance. Vishay’s MC AT Professional and Precision resistors are designed to deliver stable performance in such applications. The new Professional series devices released today feature high-temperature performance to 175 °C for 1000 hours and high power ratings of 400 mW at an 85 °C ambient temperature. Their high-temperature capability and high power ratings allow designers to use the MC AT resistors in harsh and high-temperature environments without compromising electrical performance and reliability. The devices likewise support both designers utilizing the full power capability of the MC AT and those bound to safety margins for the benefit of improved stability. The MC AT also features a superior high pulse load capability compared to typical resistors in the same case sizes. For example, the 1206-size MC AT device features ESD robustness to 2000 V (human body model). With excellent resistivity to moisture, verified under the severe conditions of 85 °C and 85 % RH for 1000 hours, all MC AT devices are optimized to provide high reliability in harsh environments. The Precision series offers low TCRs down to ±15 ppm/K and tight tolerances of ± 0.1 %, while both new series feature an extended resistance range down to 47 Ω. In addition to AEC-Q200 compliance, the MC AT series is CECC-approved. CECC approval ensures that MC AT resistors meet a set of demanding and sophisticated short-term and long-term performance requirements as defined by EN 140401-801. Compliance with these requirements is verified through periodic audits by accredited certification bodies. Device Specification Table Overview:
Samples and production quantities of the new resistors are available now, with lead times of five to six weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.
|