Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay’s New Thin Film Chip Resistors, Aimed at Down-Hole Drilling and Aviation Applications, Feature 215 °C Maximum Operating Temperature, 25 ppm/°C TCR, and Tolerances Down To 0.05 %


RMKHT thinfilm

Products mentioned:

RMKHT
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — April 15, 2010 — A new series of wire-bondable, bare die chip resistors and resistor networks optimized for extreme high-temperature environments such as down-hole drilling and aviation applications was released today by Vishay Intertechnology, Inc. (NYSE: VSH).

The new Vishay Sfernice RMKHT wire-bondable chip resistors and resistor networks feature an operating temperature range from − 55 °C to + 215 °C, with a maximum storage temperature up to + 230 °C, an industry-first for any resistor built on thin film technology. Even with this high temperature rating, the devices feature a load life stability of 0.5 % after 1000 hours at 215 °C, as well as tight TCR and tolerance values.

Typical TCR for the new discrete resistors is 25 ppm/°C, with available tolerances down to 0.05 %. Typical tracking TCR for the resistor networks is 2 ppm/°C with a ratio tolerance as low as 0.02 %.

The RMKHT resistors and resistor networks, which have a 0.4-mm height profile, are available in footprint options from 20 mils by 20 mils to 100 mils by 200 mils and with an ohmic range of 10 Ω to 6 MΩ, depending on series. Their power ratings range from 5 mW to 100 mW or 10 mW per resistor element for the resistor networks.

The RMKHT devices feature a wire-bondable construction with aluminum pads and a metallized backside option. Custom versions (CNHT) of the devices are available on request.

Samples and production quantities of Vishay’s new RMKHT resistors and resistor networks are available now, with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword