|
For more information: Vishay Siliconix Introduces First P-Channel TrenchFET® Gen III Power MOSFET in Chipscale MICRO FOOT® Package20-V Device Features Industry’s Lowest On-Resistance From 32 mΩ at 4.5 V to 120 mΩ at 1.8 V in Ultra-Small 1.5-mm by 1-mm Footprint Area
MALVERN, PENNSYLVANIA — April 26, 2010 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced the first p-channel TrenchFET® Gen III power MOSFET in the chipscale MICRO FOOT® package. The 20-V device features the industry’s lowest on-resistance for a p-channel MOSFET in the 1.5-mm by 1-mm footprint area. The new Si8499DB is the first chipscale product built on TrenchFET Gen III p-channel technology. This leading-edge technology allows a superfine, sub-micron pitch process that cuts the industry’s best on-resistance for a p-channel MOSFET by up to half. Vishay’s TrenchFET Gen III p-channel technology allows the Si8499DB to offer ultra-low on-resistance of 32 mΩ at 4.5 V, 46 mΩ at 2.5 V, 65 mΩ at 2 V, and 120 mΩ at 1.8 V. These values are 50 % lower at 4.5 V and 35 % lower at 2.5 V than the previously leading 20-V p-channel chipscale device. The Si8499DB combines TrenchFET Gen III p-channel technology with the maximum die size to footprint ratio of the device’s chipscale packaging, providing an ultra-low on-resistance in a very compact device. The PCB real estate required by the MICRO FOOT package is one sixth the size of the TSOP-6 while offering somewhat comparable on-resistance, thus saving space for other product features or enabling smaller end products. The MOSFET’s low on-resistance translates into lower voltage drops in load, charger, and battery switches, resulting in faster charging and longer battery life between charges in handheld devices such as cell phones, smart phones, PDAs, and MP3 players. The MOSFET is halogen-free in accordance with IEC 61249-2-21 and compliant to RoHS Directive 2002/95/EC. Samples and production quantities of the new Si8499DB TrenchFET power MOSFET are available now, with lead times of 16 weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. TrenchFET and MICRO FOOT are registered trademarks of Siliconix incorporated |