Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay’s Wet Tantalum Capacitor, Approved to New DSCC Drawing 10011, Offers High Capacitance to 72,000 μF and Maximum ESR Down to 0.035 Ω

10011 Series of Capacitors Features Glass-to-Metal Hermetic Seal for High-Reliability Applications


10011 capacitors

Products mentioned:

10011
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — May 17, 2010 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced an ultra-high-capacitance, wet tantalum capacitor approved to the new DSCC Drawing 10011. Vishay’s new DSCC 10011 device features a capacitance to 72,000 μF in the A, B, and C case codes. For high-reliability applications, the 10011 features a glass-to-metal hermetic seal, operates over a temperature range of - 55 °C to + 85 °C, to + 125 °C with voltage derating, and provides low maximum ESR down to 0.035 Ω at 1 kHz.

With a unique cathode system that provides the highest capacitance per unit volume available, the 10011 represents a major breakthrough in wet tantalum capacitor technology for high-energy applications. The device combines the inherent reliability of wet tantalum with the capacitance stability of solid tantalum to eliminate circuit impedance restrictions and dramatically increase capacitance ratings

Housed in an all-tantalum, hermetically sealed case, and manufactured to withstand high stress and hazardous environments, the new capacitor provides a unique double seal for reliable performance in low-voltage filtering and energy storage applications for demanding military and aerospace systems including weapon systems, radars, transponders, and power supplies.

The device offers capacitances from 1100 μF to 72,000 μF over a voltage range of 25 V to 125 V, and capacitance tolerances of ± 20 % standard at 120 Hz and + 25 °C. By providing designers with a new high standard for capacitance in a single device, the new capacitor enables reduction of capacitor or component count, lowers the amount of board space required, and simplifies the overall manufacturing and assembly process.

Samples and production quantities of the new 10011 wet tantalum capacitor are available now, with lead times of eight to 10 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword