|
For more information: Vishay’s New VOM452T and VOM453T High-Speed, 1-MBd Analog Optocouplers Feature Common Mode Rejection to 15kV/µs and Isolation Voltage of 3750VRMS in the Compact SOP-5 Package
MALVERN, Pa. — June 14, 2010 — Vishay Intertechnology, Inc. (NYSE: VSH) is broadening its optoelectronics portfolio with the release of two high-speed analog optocouplers in the industry-standard SOP-5 package, saving up to 75 % in PCB space compared to a DIP-8 SMD package. The new VOM452T and VOM453T feature a baud rate of 1 MBd in a low-profile package with a height of 2.0 mm. They also feature a very short propagation delay of 1 µs which is critical for applications requiring faster switching times than standard phototransistor optocouplers. The VOM452T and VOM453T 1-MBd optocouplers will be used for signal isolation in industrial communication bus lines, such as CANbus, CC-Link, and other serial interfaces. On one side of the bus line, they are connected to programmable logic controllers (PLCs) or automation controllers, which have an operator interface, and on the other side, they are connected to sensors on electrically noisy factory floors. The optocouplers protect operators from electrical shocks and protect the microprocessor within the PLC from being damaged by voltage spikes. The compact SOP-5 package is capable of providing 3750VRMS of voltage isolation. The VOM452T is rated for 1 kV/µs common mode noise immunity while the VOM453T is rated for 15 kV/µs. Samples and production quantities of the new VOM452T and VOM453T are available now, with lead times of 6 to 8 weeks for large orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.
|