|
For more information: Vishay Extends 140 CRH and 150 CRZ Series Surface-Mount Aluminum Capacitors with New Devices That Meet IPC/JEDEC J-STD-020 Soldering GuidelinesOffered in Seven Case Sizes, New 140 CRH Devices Provide High-Temperature Performance to + 125 °C, While 150 CRZ Capacitors Feature Very Low “Z” to 0.035 Ω and High Ripple Current to 1,756 mA
MALVERN, PENNSYLVANIA — July 29, 2010 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its high-temperature 140 CRH and low-impedance 150 CRZ series of surface-mount aluminum capacitors have been extended with new devices that meet the rigorous IPC/JEDEC J-STD-020 soldering guidelines for severe reflow conditions. The new capacitors offer the most severe reflow soldering profile available in seven case sizes, ranging from 10 mm by 10 mm by 10 mm to the larger 18 mm by 18 mm by 21 mm. The 140 CRH devices released today provide high-temperature performance to + 125 °C, while the 150 CRZ capacitors feature a very low “Z,” or maximum impedance at 100 kHz, of 0.035 Ω and a ripple current to 1,756 mA. As polarized aluminum electrolytic capacitors with a non-solid, self-healing electrolyte, the AEC-Q200-qualified devices are ideally suited for filtering, smoothing, buffering, and voltage decoupling applications. Typical end products will include automotive power trains and chassis electronics; industrial drives, automation, and equipment for renewable energy; SMPS units; domestic appliances and building control; and telecom equipment. The RoHS-compliant 140 CRH and 150 CRZ capacitors are charge- and discharge-proof, so there is no peak current limitation. For vibration-proof performance, the devices are offered in 4-pin and 6-pin versions. Device Specifications:
Samples and production quantities of the new capacitors are available now, with lead times of 12 to 18 weeks.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.
|