|
For more information: New Vishay Siliconix Medical MOSFETs for Implantable Applications Feature Package Dimensions Down to 1.6 mm by 1.6 mm, On-Resistance to 0.40 Ω
MALVERN, PENNSYLVANIA — Oct. 25, 2010 — Vishay Intertechnology, Inc. (NYSE: VSH) today released two new devices in its industry-first family of power MOSFETs built on an enhanced process flow with strict manufacturing process controls for implantable medical applications. The devices released today are an n- and p-channel 12 V MOSFET in the PowerPAK® SC-70 (SMMA511DJ) and a 20 V dual n-channel MOSFET in the PowerPAK SC75 (SMMB912DK). The new MOSFETs are distinguished from commercial devices by their high quality and reliability as ensured by enhanced quality control gates for every lot: statistical bin limit (SBL), yield limit (SYL), and part average testing (PAT) controls for wafers and component packages, and homogeneous reliability testing for all wafer lots. The rigorous SMM medical MOSFET process flow also includes an acceptable quality level (AQL) of 0.04%. Applications for the new MOSFETs will include load switching in drug delivery systems, defibrillators, pacemakers, hearing aids, and other implantable devices. Their very small package dimensions (2 mm by 2 mm for the SMMA511DJ, 1.6 mm by 1.6 mm for the SMMB912DK) will help save space in miniaturized medical devices, while their ultra-low on-resistance, down to 0.040Ω, will lower conduction losses and thus maximize battery life. Key device specifications are presented in the following table:
The growing Vishay Siliconix SMM medical MOSFET family includes n-channel, p-channel, and n- and p-channel pair configurations in various package sizes. Complete details are available at http://www.vishay.com/medical-mosfets/. Samples of the SMMA511DJ and SMMB912DK are available now. Production quantities will be available in Q4 2010 with lead times of 16 weeks for large orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. PowerPAK is a registered trademark of Siliconix incorporated. |
|||||||||||||||||||||||||||||