Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay Intertechnology’s New PHP Series of Precision, High-Power Thin Film Chip Resistors Offers TCR to ± 25 ppm/°C, Tolerances to ± 0.1 %, and Power Ratings of 1 W in 1206 and 2.5 W in 2512 Case Sizes


PHP

Products mentioned:

PHP
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — Jan. 27, 2011 — Vishay Intertechnology, Inc. (VSH: NYSE) today introduced the new PHP series of precision high-power thin film chip resistors. The devices feature a low absolute TCR of ± 25 ppm/°C, tolerances down to ± 0.1 %, and high power ratings from 1.0 to 2.5 W over a wide temperature range of - 55 °C to + 125 °C.

With stable film and performance characteristics of 1000 ppm at + 70 °C for 2000 hours, the devices released today are optimized for high-precision medical imaging, and industrial, telecommunications, and test and measurement instrumentation and equipment.

Featuring a high-purity ceramic substrate, the PHP series chip resistors are designed with enlarged backside terminations to reduce the thermal resistance between the topside resistor layer and the solder joint on the end users’ circuit board.

Offered in the 1206 and 2512 case sizes, the PHP series offers a resistance range from 10 Ω to 30 kΩ, with non-standard values available. The resistors feature 2x the power rating over traditional thin film chip resistors in the same case sizes, low noise of < - 30 dB, low voltage coefficients of 0.1 ppm/V, and voltage ratings from 100 V to 200 V. Available with lead (Pb)-free or lead terminations, the devices are RoHS-compliant and flame-resistant in accordance to UL 94 V-0.

Samples and production quantities of the PHP series will be available in Q1 2011, with lead times of 10 to 12 weeks for standard orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword