MENU
< Back  

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

Vishay Releases New Series of Mini Lug NTC Thermistors With Industry’s Smallest Lug Mounting Space of 65mm/ 0.1 in

NTCALUG03 Series Features Shortest Response Time of < 4 s for Accurate Surface Temperature Measurement


For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — March 10, 2011 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of a new series of Mini Lug negative temperature coefficient (NTC) thermistors with the industry’s smallest mounting space of 65 mm / 0.1 in, and shortest response time of < 4 s to provide fast and accurate measurements over a wide temperature range from − 40 C to + 125 C.

In addition to their small diameter, the NTCALUG03 thermistors feature a tiny 5.5 mm ring tongue that can be mounted with M2 screws or American studs #1 to 2. These small dimensions, when combined with the devices’ silver plated nickel conductor, result in a low thermal gradient of < 5% of ΔT for accurate surface temperature measurement in space-limited applications. The devices are optimized for housing, heat-sink, power electronics, and pipe and conductor thermal management in test and measurement equipment, appliances, and industrial equipment.

The thermistors released today offer designers a choice of electrical resistance values at + 25 C (R25) to meet the self heating, voltage output, or noise suppression needs of their application. The NTCALUG03 devices feature R25 of 10 kΩ, 12 kΩ, or 47 kΩ, with tolerances of 2 % and 3 %. The thermistors are available with an optional 1.5 mm pitch ZHR-2 connector, and offer customizable lead lengths and screw sizes, like M3 / American stud #3 to 4. The NTCALUG03 series is compliant to RoHS directive 2002/95/EC.

Device Specification Table:

Part # R25 value R25 tolerance B25/85 value B25/85 tolerance Includes connector
NTCALUG03A103H 10 kΩ 3 % 3984 K 0.5 % .
NTCALUG03A103HC 10 kΩ 3 % 3984 K 0.5 % X
NTCALUG03A103G 10 kΩ 2 % 3984 K 0.5 % .
NTCALUG03A103GC 10 kΩ 2 % 3984 K 0.5 % X
NTCALUG03A123H 12 kΩ 3 % 3740 K 1.5 % .
NTCALUG03A123HC 12 kΩ 3 % 3740 K 1.5 % X
NTCALUG03A473H 47 kΩ 3 % 3740 K 1.5 % .
NTCALUG03A473HC 47 kΩ 3 % 3740 K 1.5 % X

Samples and production quantities of the new NTC thermistors are available now, with lead times of twelve weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE
  • lang-code-JP
  • lang-code-ZH