|
For more information: Vishay Releases Industry’s First IHLP® Low-Profile, High-Current Inductor in 3232 Case Size With 4.0 mm ProfileIHLP-3232DZ-11 Features Inductance Values From 0.22 µH to 47.0 µH and Maximum DCR Down to 1.35mΩ
MALVERN, PENNSYLVANIA — Mar. 30, 2011 — Vishay Intertechnology, Inc. (NYSE: VSH) today launched a new IHLP® low-profile, high-current inductor that is the industry’s first such device in the 3232 case size. Featuring an 8.3 mm by 8.8 mm footprint and ultra-low 4.0 mm profile, the IHLP-3232DZ-11 offers high efficiency with maximum DCR down to 1.35 mΩ and a wide range of standard inductance values from 0.22 µH through 47.0 µH. With a DC/DC converter frequency range up to 1.0 MHz, the new IHLP-3232DZ-11 serves as a high-performing, space- and power-saving solution for voltage regulator module (VRM) and dc-to-dc converter applications in end products including next-generation mobile devices; notebooks, desktop computers, servers, graphic cards, portable gaming systems, personal navigation systems, personal multimedia devices, and automotive systems; low-profile, high-current power supplies and point of load (POL) converters; distributed power systems; field-programmable gate arrays (FPGAs); and high-current filters. The IHLP-3232DZ-11 offers an inductance range from 0.22 µH to 47.0 µH, a saturation current range from 2.6 A up to 22.0 A, a heat rating current range from 3.0 A to 34.0 A, and maximum DCR from 1.35 mΩ to 252 mΩ. The new inductor handles high transient current spikes without hard saturation. Packaged in an RoHS-compliant, 100 % lead (Pb)-free shielded, composite construction that reduces buzz noise to ultra-low levels, the new device is specified for an operating temperature range of – 55 °C to + 125 °C, with high resistance to thermal shock, moisture, mechanical shock, and vibration. Samples and production quantities of the new inductor are available now, with lead times of six to eight weeks for large orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. IHLP is a registered trademark of Vishay Dale Electronics, Inc. |