Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

New Vishay Siliconix Low-Voltage Analog Switches Feature Low On-Resistance Down to 0.6 Ω Maximum at 2.7 V in Space-Saving miniQFN Packages


DG2735A DG2725 DG2599 analogswitches

Products mentioned:

DG2735A
DG2725
DG2599
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — June 27, 2011 — Vishay Intertechnology,Inc. (NYSE: VSH) today released three new dual single pole double throw (SPDT) and dual double pole double throw (DPDT) CMOS low-voltage analog switches. The devices combine low-voltage operation and low on-resistance in small miniQFN packages for audio, SIM card, and multi-purpose signal switching in space-constrained portable end products.

The DG2735A and DG2725 are dual SPDT switches in the miniQFN10 package, designed for an operating range of 1.65 V to 4.3 V. With its guaranteed low 0.6 Ω maximum on-resistance at 2.7 V, and fast turn-on time of 64 ns, and turn-off time of 42 ns at 2.7 V, the DG2735A is ideal for audio output switching in receivers and speakers. The DG2725 offers typical on-resistance of 0.7 Ω at 3 V, while providing lower parasitic capacitance.

The DG2599 has an operation voltage range of 1.65 V to 5 V and can be used as a quad SPDT or dual DPDT switch. The device features the miniQFN16 package, on-resistance of 2.8 Ω typical at 3 V, and − 3dB bandwidth to 186 MHz. Both the DG2725 and DG2599 feature power off protection that guarantees < 1 µA COM1 and COM2 leakage, when V+ = 0 V and VCOM1 or VCOM2 = 4.3 V.

The new DG2735A, DG2725, and DG2599 analog switches are intended for use in consumer, computer, and communication products, including cell phones, PMPs and PDAs, modems and peripherals, computers, eBooks, and tablet products. Guaranteed compatible with 1.65 V logic, they are easily interfaced with low-voltage DSP or MCU control logic, making them well-suited for direct power from a one-cell Li-ion battery.

The devices released feature latch-up protection greater than 300 mA as tested per JESD78, thanks to Vishay’s sub-micron CMOS low-voltage process technology. They conduct signals within power rails equally well in both directions when on, and block signals up to the power supply level when off, with guaranteed break-before-make switching operation.

As a committed partner to the community and the environment, Vishay Siliconix manufactures these analog switches with lead (Pb)-free device terminations. The devices’ miniQFN packages have nickel-palladium-gold device terminations (represented by the “−E4” suffix), which meet all JEDEC standards for reflow and MSL ratings. The switches are halogen-free according to the IEC 61249-2-21 definition and compliant to RoHS directive 2002/95/EC.

Samples and production quantities of the new analog switches are available now, with lead time of 10 weeks.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword