Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay Intertechnology’s New 4-Terminal, 1 W Surface-Mount Power Metal Strip® Resistor is Industry’s First in 0612 Package Size With Resistance Range from 0.5 mΩ to 5 mΩ


WSK0612

Products mentioned:

WSK0612
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — Sept. 1, 2011 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new surface-mount Power Metal Strip® resistor that is the industry’s first 4-terminal, 1 W current sensing resistor in the compact 0612 package size to offer a very low resistance range from 0.5 mΩ to 5 mΩ.

The small size of the WSK0612 resistor allows it to replace larger current sensing resistors, saving space on the circuit board that in turn will create smaller and lighter products for the consumer. The WSK0612 is intended for current sensing, voltage division, and pulse applications in DC/DC converters for computers, VRMs for laptops, Li-Ion battery safety and management, and LCD TVs; and electronic automotive systems, including engine controls, multi-media electronics, climate controls, and anti-lock brakes.

Manufactured using proprietary techniques that result in extremely low resistance values, the WSK0612 features a durable all-welded construction with a solid metal nickel-chrome or manganese-copper alloy resistive element with low TCR (< 20 ppm/°C). Compliant to RoHS Directive 2002/95/EC, the resistor offers high-temperature performance to + 170 °C and low thermal EMF of < 3 µV/°C.

Samples and production quantities of the new resistor are available now, with a lead time of four to six weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Power Metal Strip is a registered trademark of Vishay Intertechnology, Inc.

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword