Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay Intertechnology Releases 18 New 200 V and 600 V FRED Pt® Hyperfast and Ultrafast Rectifiers With Forward Currents From 4 A to 15 A and Low Forward Voltage Drop Down to 0.95 V in TO-252AA (D-PAK)

Devices Include Industry’s First 600 V Rectifiers With > 10 A Forward Current in TO-252AA Power Package


For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, PENNSYLVANIA — Sept. 8, 2011 — Vishay Intertechnology, Inc. (NYSE: VSH) today launched 18 new 200 V and 600 V FRED Pt® Hyperfast and Ultrafast rectifiers in the TO-252AA (D-PAK) power plastic SMD package with forward currents from 4 A to 15 A. The devices combine extremely fast recovery times with low forward voltage drops and reverse charges, and include the industry’s first 600 V rectifiers in this package with forward currents greater than 10 A.

The 200 V rectifiers released today are offered with 4 A, 8 A, and 10 A forward currents, while the 600 V devices provide 5 A, 6 A, 8 A, 12 A, and 15 A forward currents. The 12 A VS-12EWH06FNx-M3 and 15 A VS-15AWL06FNx-M3, VS-15EWL06FNx-M3, VS-15EWH06FNx-M3, and VS-15EWX06FNx-M3 offer the industry’s highest forward currents for this device type in the TO-252AA package.

The 4 A to 6 A devices are optimized for use as snubber diodes in lighting applications (either ballast or HID), while the 8 A to 15 A devices are suitable for PFC boost and output diodes in telecom and desktop power supplies. Due to their high power density, the new Vishay rectifiers can replace larger SMD devices in these applications, such as those in the TO-263AB (D2PAK) package.

Part of Vishay’s hyperfast “H” and “X” series and ultrafast “L” series, the rectifiers offer designers a choice in speed and forward voltage performance to meet the needs of their application. The devices feature an improved chip design for increased reliability exceeding standard requirements for resistance to moisture and IR stability over time.

The rectifiers feature low forward voltage drops from 0.95 V at 4 A for “L” series devices. Reverse recovery times start at 17 ns (at IF = 8 A, di/dt = 200 A/µs, VR = 390 V) for the “X” series, while reverse recovery charges start at 20 nC (at IF = 4/5 A, di/dt = 200 A/µs, VR = 160 V) for the “H” series.

The rectifiers offer a max operating junction temperature of + 175 °C for a more robust and cost-effective design, and extremely low leakage current. Compliant to RoHS Directive 2002/95/EC, the devices are halogen free according to the IEC 61249-2-21 definition, and provide an MSL moisture sensitivity level of 1, per J-STD-020, LF maximum peak of + 260 °C.

Samples and production quantities of the new rectifiers are available now, with lead times of 16 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword