Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay Intertechnology Extends IHLP® Family of Low-Profile, High-Current Inductors With New Device in the 3232 Case Size

IHLP-3232CZ-11 Features Ultra-Low 3.0 mm Profile, Inductance Values From 0.22 µH Through 33.0 µH, and Maximum DCR Down to 1.62 mΩ


IHLP-3232CZ-11 inductors

Products mentioned:

IHLP-3232CZ-11
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — Sept. 19, 2011 — Vishay Intertechnology, Inc. (VSH: NYSE) today launched a new IHLP® low-profile, high-current inductor in the 3232 case size. Featuring an 8.26 mm by 8.79 mm footprint and ultra-low 3.0 mm profile, the compact IHLP-3232CZ-11 offers high efficiency with maximum DCR down to 1.62 mΩ and a wide range of standard inductance values from 0.22 µH through 33.0 µH.

With a frequency range up to 1 MHz, the new IHLP-3232CZ-11 serves as a high-performing, space- and power-saving solution for voltage regulator module (VRM) and dc-to-dc converter applications in end products including next-generation mobile devices; notebooks, desktop computers, servers, graphic cards, portable gaming systems, personal navigation systems, personal multimedia devices, and automotive systems; low-profile, high-current power supplies and point of load (POL) converters; distributed power systems; and field-programmable gate arrays (FPGAs).

The IHLP-3232CZ-11 offers an inductance range from 0.22 µH to 33.0 µH, a saturation current range from 2.5 A up to 24.0 A, a heat rating current range from 2.6 A to 36.0 A, and maximum DCR from 1.62 mΩ to 205.0 mΩ.

The new inductor handles high transient current spikes without hard saturation. Packaged in an RoHS-compliant, 100 % lead (Pb)-free shielded, composite construction that reduces buzz noise to ultra-low levels, the device is specified for an operating temperature range of −55 °C to + 125 °C, with high resistance to thermal shock, moisture, mechanical shock, and vibration.

Samples and production quantities of the new inductor are available now, with lead times of 10 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

IHLP is a registered trademark of Vishay Intertechnology, Inc.

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword