Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

New Vishay Siliconix CMOS Analog Switch and Multiplexers Feature Wide 2.7 V to 16 V Single-Supply and ± 2.7 V to ± 8 V Dual-Supply Voltage Range

Offering Outstanding Performance in Ultra-Compact MiniQFN Packages, Devices Provide Low-Voltage Logic Compatibility Down to 1.4 V


DG9236 DG9251 DG9252 DG9253 analogswitches

Products mentioned:

DG9236
DG9251
DG9252
DG9253
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — Oct. 17, 2011 — Vishay Intertechnology, Inc. (VSH: NYSE) today expanded its DG92xx family of CMOS analog switching and multiplexer products with the introduction of four new devices designed for 2.7 V to 16 V single-supply or ± 2.7 V to ± 8 V dual-supply operation. The new devices combine their wide voltage range operation with compact package sizes and low-voltage logic compatibility for high-speed, high-precision switching applications.

The products released today include a dual SPDT analog switch (DG9236), an 8-channel multiplexer (DG9251), a dual 4-channel multiplexer (DG9252), and a triple 2-channel multiplexer (DG9253). The new devices are optimized for touch panels, tablets, data acquisition, healthcare, instrumentation, and automation equipment.

The DG9251, DG9252, and DG9253 are fully specified at + 16 V, + 5 V and ± 5 V. Compatible with CMOS and GPIO control signals, the devices’ control inputs have guaranteed 1.4 V logic high when operating from + 5 V or ± 5 V supplies, and 1.65 V logic high when operating from a + 16 V supply. For CMOS/TTL microprocessor control signals, the DG9236 has a guaranteed 1.8 V logic high when operating from a +16 V power supply.

The three multiplexers are offered in the compact 1.8 mm by 2.6 mm miniQFN-16 package, while the DG9236 analog switch is offered in the 1.4 mm by 1.8 mm miniQFN-10 package with a low 0.55 mm profile. The devices’ plastic miniQFN packages are the smallest in the industry, and are comparable to WCSP type packages.

At − 3 dB, the multiplexers offer a bandwidth of 314 MHz (DG9251), 449 MHz (DG9252), and 480 MHz (DG9253), and provide excellent isolation performance of - 45 dB (typical) at 100 MHz and crosstalk of − 48 dB (typical) at 100 MHz. The DG9236 features a bandwidth of 800 MHz and - 70 dB crosstalk and − 62 dB off-isolation at 10 MHz. All four devices are specified for an operating temperature range of - 40 °C to + 85 °C.

Fabricated using Vishay’s proprietary CMOS process, the switch and multiplexers feature low parasitic capacitance, charge injection, leakage current, and power consumption. Designed to handle a wide range of analog and high-speed pulses, the devices conduct equally well in both directions, offer rail-to-rail analog signal handling, and can be used as both multiplexers and de-multiplexers.

As a committed partner to the community and the environment, all analog switches and multiplexers manufactured by Vishay Siliconix are compliant to RoHS directive 2002/95/EC and halogen-free in accordance to the IEC 61249-2-21 definition. The miniQFN family of packages features nickel-palladium-gold device terminations that meet all JEDEC standards for reflow and MSL rating.

Samples and production quantities of the new analog switch and multiplexers are available now, with lead times of 10 weeks for standard orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword