Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Vishay Intertechnology Releases Industry’s First CAT IV, High-Voltage Isolation Optocouplers in Surface-Mount Packages for Solar and Wind Turbine Installations

Devices Are VDE Certified for CAT IV Installations With Transient Overvoltage Protection of 12,000 V and Recurring Peak Voltage of 1,450 VPEAK


For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com


This release in:

MALVERN, Pa. — Oct. 24, 2011 — Vishay Intertechnology, Inc. (VSH: NYSE) today broadens its optoelectronics portfolio with the introduction of the industry’s first CAT IV, high-voltage isolation optocouplers available in surface-mount packages. Certified by the international safety regulatory agency VDE, the CNY64ST and CNY65ST series products offer long creepage distances and a high isolation test voltage to protect workers and equipment used in high-voltage environments like solar power and wind turbine grid connections. Now customers wanting the manufacturing flexibility of using all surface-mount components in their products can use the CNY64ST and CNY65ST, which complement the CNY6x series of through-hole devices already available.

The International Electrotechnical Commission (IEC) has defined protection standards for four different installation categories, CAT I through IV. Category IV has the most stringent protection requirements because it typically involves electrical connections to the utility grid. The CNY6x series of CAT IV optocouplers protects equipment and people from being damaged or injured by a high-voltage spike or transient of up to 12,000 V and a recurring peak voltage of 1450 VPEAK, while allowing data to pass from the high-voltage side to low-voltage monitoring equipment.

In addition to meeting the IEC requirements for overvoltage transients and recurring peak voltage, the CNY6x series of optocouplers features creepage distances — the shortest distance along any path on the outside surface of the package from input to output pin — of up to 17 mm and is certified to be used in CAT IV installations with working voltages up to 1,000 V.

For the surface-mount devices released today, the CNY64ST series offers a creepage distance of 9.5 mm while the CNY65ST series provides a creepage distance of 14 mm with CAT IV working voltages up to 600 V. Both feature an insulation distance — the internal distance between the infrared emitting diode and phototransistor through the insulation — greater than 3 mm.

The CAT IV optocouplers provide a broad range of CTR values from 50 % to 300 % at 5 mA, operate over a temperature range of − 55 °C to + 85 °C, and offer a forward current of 75 mA. The devices are Eco-Friendly “Green,” compliant to RoHS Directive 2002/95/EC, and in accordance to WEEE 2002/96/EC.

Samples and production quantities of the CNY64ST and CNY65ST series products are available now, with lead times of six to eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword