|
For more information: Vishay Intertechnology’s New 4-Line Bus Port Protection Array Provides Low Typical Capacitance of 0.6 pF and Leakage Current of < 0.1 µA in New Ultra-Compact LLP2510 Package Featuring Low 0.55 mm Profile
MALVERN, Pa. — Nov. 7, 2011 — Vishay Intertechnology, Inc. (VSH: NYSE) today released a new 4-line ESD-protection array in the new ultra-compact LLP2510 package. Featuring a compact 2.5 mm by 1.0 mm footprint and ultra-low profile of 0.55 mm, the VBUS54ED-FBL offers low capacitance and leakage current for the protection of high-speed data lines against transient voltage signals. In addition to saving board space, the 4-line VBUS54ED-FBL features a “flow through” design that supports the surge resistance requirements for high-speed data lines in applications such as USB 3.0, HDMI, DisplayPort, eSATA, and 1394/Firewire in mobile electronics including notebook computers, cell phones, MP3 players, and portable gaming systems. The new device features a low load capacitance of 0.6 pF and a low maximum leakage current of < 0.1 µA at the working voltage of 5.5 V. The array offers a breakdown voltage of typical 7.9 V at 1 mA, and a maximum clamping voltage of 12.5 V at 2 A. The VBUS54ED-FBL provides transient protection for data lines as per IEC 61000−4−2 (ESD) at 15 kV (air and contact discharge). The lead (Pb)-free device is compliant with RoHS 2002/95/EC and WEEE 2002/96/EC, and its soldering can be checked by standard vision inspection without X-rays. Samples and production quantities of the new VBUS54ED-FBL are available now, with lead times of eight to 10 weeks for large orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.
|