Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay Intertechnology Introduces New MIL-PRF-83401-Qualified Single-in-Line Thin Film Resistor Network

Available in 6-, 8-, and 10-Pin Configurations, Device Features TCR of ± 25 ppm/°C and Tight Ratio Tolerances to ± 0.05 %


120209arrays

Products mentioned:

M83401
C83401
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — Feb. 9, 2012 — Vishay Intertechnology, Inc. (VSH: NYSE) today introduced a new MIL-PRF-83401-qualified (cage code 57489) through-hole, single-in-line thin film resistor network. Featuring low absolute TCR of ± 25 ppm/°C, TCR tracking of 5 ppm/°C, and tight ratio tolerances to ± 0.05 %, the M83401 will outperform all the requirements of MIL-PRF-83401 R, V, and H characteristics.

The resistor network released today offers three to nine resistors, and is available in 6-, 8-, and 10-pin low-profile configurations in isolated (G) and pin one common (C) schematic styles. The type RZ070, RZ080, RZ090, RZ210, RZ220, and RZ230 device features 100 % burn-in screening for increased reliability in demanding military applications.

The M83401 features Vishay Dale Thin Film’s patented SPM passivated Tamelox film for very low noise of < - 30 dB, voltage coefficient of < 0.1 ppm/V, power ratings from 0.06 mW to 0.120 mW per element (0.18 W to 1.0 W per package), and a wide resistance range of 100 Ω to 200 kΩ per resistor. The device operates over a temperature range of - 55 °C to + 125 °C.

Offering a low 4.95 mm (0.197 in) maximum seated height, the resistor network features a rugged, molded thermoset plastic construction with gold-plated copper alloy leads. The leads are attached to the metallized alumina substrates by thermocompression bonding. The M83401 is also available in a commercial version: the C83401.

Samples of the M83401 and C83401 resistor networks are available now. Production lead times are 12 to 14 weeks for standard orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword