Vishay Intertechnology’s IWAS-4832FF-50 Wireless Charging Receiving Coil, RFCS Capacitors, 20 LHE Hall Effect Sensor, and VLMx1300 LEDs Selected for Electronic Design’s Annual “Top 101 Components”


Top 101 Components
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

MALVERN, Pa. — July 5, 2012 — Vishay Intertechnology, Inc. (NYSE:VSH) today announced that the company’s IWAS-4832FF-50 wireless charging receiving coil, RFCS thin film RF capacitors, 20 LHE Hall effect linear position sensor, and VLMx1300 LEDs have been selected for Electronic Design’s “Top 101 Components.” The annual list compiles the 101 most popular components from the previous year among readers of the magazine’s Products of the Week newsletter.

#9 − IWAS-4832FF-50 Wireless Charging Receiving Coil

For wireless power base stations and receivers, the IWAS-4832FF-50 is the industry’s first commercially available powdered-iron-based, WPC-compliant (Wireless Power Consortium) wireless charging receiving coil optimized for use with or without an alignment magnet. Offering a durable construction and high permeability shielding, the new IWAS-4832FF-50 provides high efficiency for wireless charging of portable electronics.

Link to product datasheet:

http://www.vishay.com/doc?34311 (IWAS-4832FF-50)

#55 − RFCS Thin Film RF Capacitors

Vishay’s RFCS surface-mount thin film RF capacitors offer the industry’s highest self-resonance frequency for this device type, which ranges from 8.5 GHz to 20 GHz. The capacitors are ideal for impedance matching circuits, decoupling, DC blocking, and other circuit applications in end products with operating frequencies greater than 5 GHz.

Link to product datasheet:

http://www.vishay.com/doc?61090 (RFCS)

#57 − 20 LHE Hall Effect Linear Position Sensor

The 20 LHE linear position sensor covers short electrical strokes to 10 mm max and is available with a spring return system. The device’s Hall effect technology gives it the ability to perform in conditions involving high-frequency vibrations up to 20 G and shocks up to 50 G. With a long life of 10 million cycles, the device is ideal for short stroke measurements in industrial applications.

Link to product datasheet:

http://www.vishay.com/doc?57115 (20 LHE)

#62 − VLMx1300 LEDs

The VLMx1300 series of super-thin, ultra-bright LEDs in the small SMD 0603 package uses an innovative ChipLED technology. Available in super red, soft orange, yellow, yellow green, true green, blue, and white, the devices are mounted on highly reliable PCBs measuring 1.6 mm x 0.8 mm x 0.55 mm.

Link to product datasheet:

http://www.vishay.com/doc?82437 (VLMS1300, VLMO1300, VLMY1300, VLMG1300, VLMTG1300, VLMB1300, VLMB1310)

http://www.vishay.com/doc?82435 (VLMW1300)

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.