About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay Intertechnology Launches New Ultraviolet LED in PLCC-2

New Solid-State Device Replaces Mercury Vapor Lamps in Production Curing Operations


VLMU3100 leds

Products mentioned:

VLMU3100
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

This release in:

MALVERN, Pa. — Oct. 25, 2012 —The Optoelectronics group of Vishay Intertechnology, Inc. (NYSE: VSH) today announced the VLMU3100, an ultraviolet (UV) LED in the surface-mount PLCC-2 package. Aimed at a wide range of applications, including adhesive curing, the VLMU3100 will serve as a solid-state replacement for mercury vapor lamps.

The VLMU3100 features a typical luminous intensity of 11 mcd at 20 mA, with a typical wavelength of 405 nm and forward voltage of 3.2 V for low power consumption.

Designed for long service life, the VLMU3100’s PLCC-2 package consists of a lead frame which is embedded in a white thermoplastic. The reflector inside this package is cast in clear silicone, guaranteeing a long lifetime. The viewing angle is 120°, and the package dimensions are 3.2 mm by 2.8 mm by 1.9 mm.

The VLMU3100 overcomes many of the problems associated with systems based on mercury vapor lamps, which generate significant heat and degrade unpredictably over their service lives. By comparison, the VLMU3100 features power dissipation of just 120 mW and all the benefits of solid-state LED technology to ensure reliable and stable performance.

The VLMU3100’s EIA- and ICE-standard PLCC-2 package is compatible with IR reflow and vapor phase soldering. The devices are supplied in 8 mm tape for automatic placement equipment.

Samples and production quantities of the VLMU3100 are available now, with lead times of four to six weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword