Vishay Intertechnology’s Si7655DN MOSFET Named as 2013 Product of the Year by Electronic Products China Magazine

-20 V P-Channel Device Offers Industry-Low RDS(ON) of 4.8 mΩ at 4.5 V in Ultra-Slim PowerPAK® 1212-8S Package.


EPC
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

MALVERN, Pa. — April 8, 2014 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its Si7655DN MOSFET was chosen as a winner in Electronic Products China magazine’s sixth annual Product of the Year Awards. The Si7655DN is the industry’s first -20 V p-channel MOSFET in a 3.3 mm by 3.3 mm package to offer on-resistance of just 4.8 mΩ maximum at a 4.5 V gate drive, and the first device to be released in a new version of the Vishay Siliconix PowerPAK® 1212 package.

The editors of Electronic Products China evaluated hundreds of products launched in China's electronics market in 2013 on the basis of innovative design, significant advancement in technology or application, and substantial achievement in price and performance. Vishay’s Si7655DN MOSFET was selected because of its demonstrated success in the MOSFET category.

Utilizing the new PowerPAK 1212 package version and Vishay Siliconix’s industry- leading p-channel Gen III technology, the Si7655DN provides industry-low maximum on-resistance of 3.6 mΩ (-10 V), 4.8 mΩ (-4.5 V), and 8.5 mΩ (-2.5 V). These specifications represent an improvement of 17 % or better over the next best competing -20 V devices.

The low on-resistance of the Si7655DN allows designers to achieve lower voltage drops in their circuits and promotes more efficient use of power and longer battery run times. Compared to the PowerPAK 1212, the device's PowerPAK 1212-8S package provides a 28 % slimmer nominal profile of 0.75 mm to save valuable board space, while maintaining the same PCB land pattern.

Link to product datasheet:

http://www.vishay.com/doc?63617

The Electronic Products China 2013 Product of the Year Award winners were announced in the February 2014 issue of the magazine. The complete list of winners, in Chinese, is available at http://www.21ic.com/wz/CRXDQWHFA/20140202/20140202.htm.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.