New Vishay Intertechnology Polymer Tantalum Chip Capacitors Offer Ultra-Low ESR in Compact J, P, A, B, and Low-Profile B Case Sizes

Devices Offer Wide Capacitance Range From 3.3 F to 330 F for Computer, Telecom, and Industrial Applications


T55

Products mentioned:

T55
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
MALVERN, Pa. — Dec. 9, 2014 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new vPolyTan™ series of surface-mount polymer tantalum molded chip capacitors in five compact case sizes. Optimized for computer, telecom, and industrial applications, Vishay Polytech T55 series devices feature ultra-low ESR down to 30 mΩ at +25 C and 100 kHz.

The low ESR of the capacitors released today is a result of their polymer cathodes, which offer greatly enhanced performance over manganese dioxide devices. In addition, the T55 series offers excellent ripple current rating up to 1.78 A IRMS and provides low equivalent series resistance (ESR) for enhanced charge and discharge characteristics. The capacitors will be used for power management, battery decoupling, and energy storage in computers, tablets, smart phones, and wireless cards.

Offered in the J, P, A, B, and T (low-profile B − 1.2 mm max.) case sizes, T55 series devices feature a wide capacitance range from 3.3 F to 330 F over voltage ratings from 2.5 V to 10 V, and a capacitance tolerance of 20 %. The devices operate over a temperature range of -55 C to +105 C with voltage derating above +85 C.

Featuring lead (Pb)-free terminations, T55 series capacitors are RoHS-compliant, halogen-free, and Vishay GREEN. The devices are compatible with high-volume automatic pick-and-place equipment and offer a Moisture Sensitivity Level (MSL) of 3.

Resources:

Product datasheet on the Vishay website

Check distributor stock on the Vishay website

Weekly updates: sign up for Vishay Newsfeed

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

vPolyTan is a trademark of Vishay Intertechnology, Inc.