Vishay Intertechnology Dual Inductor Saves Space, Offers Industry-High Temperature Range for Class D Amplifiers


Inductor

Products mentioned:

IHLD-4032KB-5A
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
MALVERN, Pa. — Feb. 24, 2015 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced the first device in its new IHLD series of low-profile, high-current dual inductors. Offering two inductors in one 4032 package, the space-saving, automotive-grade IHLD-4032KB-5A is the industry's first dual inductor to offer a high operating temperature range to +155 C.

The Vishay Dale inductor released today is optimized for automotive and commercial class D amplifier circuits, where the device reduces board space requirements and offers improved performance over using multiple discrete inductors. The IHLD-4032KB-5A's optimal design produces high-quality sound, low distortion, and low coupling for minimal cross-talk between inductors.

Built on Vishay's IHLP technology, the AEC-Q200-qualified inductor offers max. DCR from 32.6 mΩ to 107 mΩ, inductance from 10 H to 33 H, rated current to 5.6 A, and a frequency range up to 1 MHz. The device handles high transient current spikes without saturation and has excellent temperature stability for inductance and saturation over its operating range. Manufactured using a 100 % lead (Pb)-free shielded, composite construction package, the IHLD-4032KB-5A is specified for an operating temperature range of -55 C to +155 C, with high resistance to thermal shock, moisture, mechanical shock, and vibration

Samples and production quantities of the new dual inductor are available now, with lead times of 10 to 12 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

IHLP is a registered trademark of Vishay Intertechnology